Technical FAQs

Ask a Question

What are the different ways user interface VAMP 255/245/230 relay's can be controlled.

The relay can be controlled in three ways:
> Locally with the push-buttons on the relay front panel
> Locally using a PC connected to the serial port on the front panel or on the rear panel of the relay (both cannot be used simultaneously)
> Via remote control over the remote control port on the relay rear panel.
Was this helpful?
What can we do to improve the information ?