Technical FAQs

Ask a Question

How to enable NTP (Network Time Protocol) service in BMXNOC0401 module.

NTP services can be activated for BMXNOC0401 from DTM browser in Unity Pro. You have to follow below path :-
Unity Pro >> Tools >> DTM Browser >> M_NOC0401.2 >> Services >> NTP (Select here Enable / Disable )

Operation of the network time service can be monitored and diagnosed in:
- the Network Time Service Diagnostics page of the Unity Pro software, and
- the Network Time Service web page embedded in BMXNOC module.

PLease note  :- The network time service is available only when you first perform the following tasks:
- upgrade the firmware in the BMX NOC 0401 Ethernet communication module to version 2.01 or higher
- select the BMX NOC 0401.2 Ethernet communication module for your project using Unity Pro version 7.0 or higher
 
Was this helpful?
What can we do to improve the information ?