Technical FAQs

Ask a Question

What is the frequency of NTP time synchronization in BMXNOC0401.2 module.

The frequency the Ethernet communication module NOC0401.2 uses for requesting a time setting from the NTP server can be in between 1...120 seconds. By default this value is euqal to 18 sec.
Was this helpful?
What can we do to improve the information ?