Technical FAQs

Ask a Question

Can i use more than one 140NOC78100 in Quantum ERIO architecture.

A Quantum ERIO local rack contains one 140 CRP 312 00 remote I/O head module and can have upto 6 communication modules but only one of which can be a 140 NOC 781 00 control head module.
Was this helpful?
What can we do to improve the information ?