Technical FAQs

Ask a Question

Which frequency range is suitable for RXM plug in relays to work properly.

The relays are qualified and expected to operate on networks with 50Hz and 60Hz. There is no particular accuracy required from the products. It`s AC coils are qulaified to work for network at 50Hz / 60Hz
Was this helpful?
What can we do to improve the information ?