Technical FAQs

Ask a Question

What are the dimensions of LCD dot matrix display and it's purpose in VAMP 255/245/230 relay's.

The relay is provided with a backlightedt 128x64 LCD dot matrix display.

The display has two different purposes: one is to show the single line diagram of the relay with the object status, measurement values, identification
etc. The other purpose is to show the configuration and parameterization values of the relay.
Was this helpful?
What can we do to improve the information ?