Technical FAQs

Ask a Question

Is it possible selecting trigger input for backlight control in VAMP 255/245/230 relay's.

Display backlight can be switched on with a digital input, virtual input or virtual output. LOCALPANEL CONF/Display backlight ctrl setting is used for selecting trigger input for backlight control. When the selected input activates (rising edge), display backlight is set on for 60 minutes.
Was this helpful?
What can we do to improve the information ?