Technical FAQs

Ask a Question

How to reset password to the default values for VAMP 255/245/230 relay's if lost.

Password handling
The passwords can only be changed using VAMPSET software connected to the local RS-232 port on the relay.
It is possible to restore the password(s) in case the password is lost or forgotten. In order to restore the password(s), a relay
program is needed. The serial port settings are 38400 bps, 8 data bits, no parity and one stop bit. The bit rate is
configurable via the front panel.
Command               Description
get pwd_break         --> Get the break code (Example: 6569403)
get serno Get          --> the serial number of the relay (Example: 12345)

Send both the numbers to country customer care center and ask for a password break. A device specific break code is sent back to you. That code will be valid for the next two weeks.
Command                          Description
set pwd_break=4435876 --> Restore the factory default passwords (“4435876” is just an example. The actual code should be asked from VAMP Ltd.)
Now the passwords are restored to the default values.
Was this helpful?
What can we do to improve the information ?