Technical FAQs

Ask a Question

Can we use the Serial communication using Unitelway driver for Premium PLC and Vijeo Citect`s 7.40 version .

Yes you can still able to use the "UNITEL" protocol with VJC v7.30/7.40. This Unitel protocol is still available in this current VJC versions also. 
Was this helpful?
What can we do to improve the information ?