Technical FAQs

Ask a Question

Can we use both RS 232 ports available for connecting a local PC with VAMPSET to the VAMP 255/245/230 relay's at the same time.

Two RS 232 serial ports are available for connecting a local PC with VAMPSET to the relay; one on the front panel and one on the rear panel of the relay. These two serial ports are connected in parallel. However, if the connection cables are connected to both ports, only the port on the front panel will be active.
Was this helpful?
What can we do to improve the information ?