Technical FAQs

Ask a Question

Is it possible to connect VAMPSET program using TCP/IP LAN connection in VAMP 255/245/230 relay's.

The VAMPSET program can also use TCP/IP LAN connection. Optional hardware is required.
Was this helpful?
What can we do to improve the information ?