Technical FAQs

Ask a Question

What is the limit to the scope of inverse curves with high pick-up settings in for protection function overcurrent state I> (50/51) VAMP 255/245/230 relays.

The maximum measured secondary current is 50xIN. This limits the scope of inverse curves with high pick-up settings.
 
Was this helpful?
What can we do to improve the information ?