Technical FAQs

Ask a Question

With Vijeo Historian V4.50 installation we do not have any excel client installed on system. How can I install the excel client .

With new Vijeo Historian Version 4.50 the excel client is replaced with new featured Historian Enquire, which needs to be installed separately from the 
installation DVD or from Launch .exe. In the installation DVD you will find a "Historian Enquire.exe" , you need to run that exe file to install this enquire. 
Was this helpful?
What can we do to improve the information ?