Technical FAQs

Ask a Question

How can I display all my alarms (from my different clusters) on a single alarm page in Vijeo Citect.


If you configure alarms from different clusters, you will be able to display them all on a singel alarm page by calling 

AlarmDsp(250, 25, 0) ->the 4th argument ("cluster") is not specified, so all alarms will be displayed by default.This is the case in the CSV_Include alarm page for instance.

 If you wish to "filter" your alarms by cluster, you will simply need to dynamically set the cluster argument to which ever cluster you wish.

For example: AlarmDsp(250, 25, 0, "ClusterOne").

 
Was this helpful?
What can we do to improve the information ?