Technical FAQs

Ask a Question

What are the probable causes of CFF in Altivar 32 drive.

CFF means incorrect configuration.
Following are the probable cause:
  • Option card changed or removed.
  • Control block replaced by a control block configured on a drive with a different rating.
  • The current configuration is inconsistent
Was this helpful?
What can we do to improve the information ?