Technical FAQs

Ask a Question

How to size the contactor when it is used for the controlling the passive filter via the drive according to the load.

The contactor has to be in category AC1 sized at 50% of the nominal current (In) of passive filter [Not drive nominal current (In)].
Was this helpful?
What can we do to improve the information ?