Technical FAQs

Ask a Question

what is the maximum motor cable length for Altivar 12 without motor choke.

Maximum motor cable length for Altivar 12 without motor choke is 50m (shielded cable) and 100m (unshielded cable).
Was this helpful?
What can we do to improve the information ?