Technical FAQs

Ask a Question

what is the maximum motor cable length for Altivar 32 without motor choke.

Maximum motor cable length for Altivar 32 without motor choke is 10m (shielded cable) and 50m (unshielded cable).
Was this helpful?
What can we do to improve the information ?