Technical FAQs

Ask a Question

How many single contacts can be added behind the selector switch ZA2BD3 for front mounting on Harmony XAC-A Pendant Control Station Enclosure.

For space constraint, It is possible to add maximum two numbers of single block contact block ZB2BE101 OR ZB2BE102 (side by side mounting) behind a 3 position selector switch ZA2BD3 operator for front mounting on Harmony XAC-A Pendant Control Station Enclosure.
Was this helpful?
What can we do to improve the information ?