Technical FAQs

Ask a Question

What are the motor thermal states when OLF (Motor OverLoad) fault set & reset on Altivar 71 drive.

The OLF fault is set when the motor thermal state (tHr) is higher than 118%.
The OLF fault is reset when the motor thermal state (tHr) is lower than 100%.
Was this helpful?
What can we do to improve the information ?