Technical FAQs

Ask a Question

What is the difference between XCKJ432009 & XCKJ167 limit switch.

The XCKJ432009 unit is a specific product for radioactive ambient and based on XCKJ167. These dimensions are identical. 
XCKJ432009 limit switch is special for nuclear applications and the different tests were made by the SGN organism. 

Main technical characteristics of XCKJ432009: 
  • Operation temperature: 10°C ....+ 100°C 
  • Irradiated resistance: 5MGy 
  • Operation: ambient no corrosive without water splashing 
  • Degree of protection: IP57 on no irradiated product
Was this helpful?
What can we do to improve the information ?