Technical FAQs

Ask a Question

What to do when "Remote Connection" Tab remains diabled in SoMachine

"Remote Connection" tab diablity in SoMachine is generallly seen with Windows 7 - 32 / 64 bit operating system mainly because of UAC (User account control) settings

Go to Control Panel. Open User Accounts. Click on "Change User Account Control" settings.
Make setting of UAC to "Never Notify". Re-start your system.
User should get "Remote Connection" tab activated with SoMachine.

Was this helpful?
What can we do to improve the information ?