Technical FAQs

Ask a Question

Is it mandatory to import ATV71 - GSD file to PLC (profibus Master) configurations when ATV71+Profibus DP card is used to Interchangeability mode to support ATV58+Profbus migration

Profibus DP card VW3A3307 -  DIP switch 1 is made to ON position of ATV58 Interchangeability mode, controller will see ATV71 as ATV58 and there is no need to modify the PLC application / configuration . No need to import GSD file of ATV71
Was this helpful?
What can we do to improve the information ?