Technical FAQs

Ask a Question

Is it possible to order Altivar 71 greater than 75 KW without DC choke.


Altivar 71 greater than 75 KW Drive supplied as standard with a DC choke, which must be used when connecting the drive to the three-phase supply.
Yes, it is possible to order Altivar 71 greater than 75 KW without DC choke by adding a D at the end of the reference.
For example: ATV71HD90N4 becomes ATV71HD90N4D.
Was this helpful?
What can we do to improve the information ?