Technical FAQs

Ask a Question

Is Altivar 71 drive comply Voltage dips & short interruptions standard.

Altivar 71 drives comply with IEC61800-3 standard, which contains the IEC61000-4-11 (Testing and measurement techniques – Voltage dips, short interruptions and voltage variation immunity tests).
Was this helpful?
What can we do to improve the information ?