Technical FAQs

Ask a Question

Do we need to do Dielectric & insulation test for Altivar 71 drives.

We made a Dielectric & insulation test during the final test after manufacturing of ATV need to do these tests.
However, for information, please find the detail of dielectric test in attachment and Regarding Insulation resistance test, For all ATV ranges of drives should carry a insulation resistance test between power terminal (A) and ground @ 500VDC for 1 min. and should get value of >= 1 M OHM 
Note: Power Terminal is same "A" as per the dielectric test.
Was this helpful?
What can we do to improve the information ?