Technical FAQs

Ask a Question

What is the surge capability of Altivar 71 drive.

The VSD ATV71/61 passes an immunity test. It consists in testing the immunity of VSD with unidirectional surges .This test comply with IEC 61000-4-5 standard. The test done are the Surge of 1.2/50µs,1KV Line to Line and 2kV Line to ground.
Was this helpful?
What can we do to improve the information ?