Technical FAQs

Ask a Question

What is the tripping class of EasyPact TVS LRE*** thermal overload relays.

The tripping class of EasyPact TVS LRE*** thermal overload relays is Class 10A conforming to IEC 60947-4-1.
Was this helpful?
What can we do to improve the information ?