Technical FAQs

Ask a Question

What is the Dielectric strength of EasyPact TVS LRE*** thermal overload relays.

The Dielectric strength of EasyPact TVS LRE*** thermal overload relays at 50Hz is 6kV Conforming to IEC 60801-5.
Was this helpful?
What can we do to improve the information ?