Technical FAQs

Ask a Question

What is the vibration resistance of EasyPact TVS LRE*** thermal overload relays.

The vibration resistance of EasyPact TVS LRE*** thermal overload relays is 3 gn permissive acceleration conforming to IEC 60068-2-6.
Was this helpful?
What can we do to improve the information ?