Technical FAQs

Ask a Question

What is the shock resistance of EasyPact TVS LRE*** thermal overload relays.

The shock resistance of EasyPact TVS LRE*** thermal overload relays is 6 gn - 11 ms permissive acceleration conforming to IEC 60068-2-7.
Was this helpful?
What can we do to improve the information ?