Technical FAQs

Ask a Question

What are the components for XCKS159 limit switch.


The components for XCKS159 Limit switch are ZCKS1 body + ZCKD59 lever
ZCKS1=>Body with 2-pole contact, cable entry for Pg 13.5 1
ZCKD59=>Round rod lever, thermoplastic, Ø 6 mm, L = 200 mm
Was this helpful?
What can we do to improve the information ?