Technical FAQs

Ask a Question

What is the part number & feature of SCP for Conext XW inverter.

SCP is System Control Panel and part number is 865-1155.
The SCP features a graphical, backlit LCD display providing system configuration and diagnostic information for devices connected to the XanbusTM enabled network. The SCP gives a single point of control to setup and monitor an entire system, which may consist of multiple Conext inverter/chargers, MPPT solar charge controllers and other components.
Was this helpful?
What can we do to improve the information ?