Technical FAQs

Ask a Question

Why is the input current smaller than the output current on Altivar 212 drive catalogue.

The Output current is with THDI=0% (no harmonic). Only fundamental current.
The input current is with THDI>0 % => so, the Line current on this case is the fundamental current with harmonic current.
The harmonic causes that the input current is less than output current. 
Was this helpful?
What can we do to improve the information ?