Technical FAQs

Ask a Question

Is the HMIGTO2310 or other HMIGTO series compliant with Hazardous Area standard Class I Division 2.

Yes our HMI GTO series and below model are complaint to UL Certification Class I, Division 2 :

HMIGTO6310, HMIGTO6315, HMIGTO5310, HMIGTO5315, HMIGTO4310, HMIGTO3510, HMIGTO2310, HMIGTO2315, HMIGTO2300, HMIGTO1310, HMIGTO1300.
Was this helpful?
What can we do to improve the information ?