Technical FAQs

Ask a Question

With Vijeo Citect 7.40 what are the new functions available to read XML file.

To read data from a XML file we need to use some of the new available inbuilt XML functions of VJC 7.40 like XMLCreate,XMLGetAttribute, XMLGetChildCount  XMLGetAttributeCount, XMLGetChild etc. You need to use these functions to read the data from parent node and then need to run a loop for the Child node also . There is no defined procedure to read these XML file , we need to write a customized cicode each and every XML file. You will get more details in the help files for these functions in the attached file. 
Was this helpful?
What can we do to improve the information ?