Technical FAQs

Ask a Question

We have to poll tag data for specified time interval from Vijeo Citect to our PLC device. How can I configure it.

You can use the inbuilt function of Vijeo Citect "IODeviceControl" to disable the IO Device . Using this "IODeviceControl"  function you can enable the IO Device and update the tag values and then disable the IO Device again and also during the time when the IO Device is disable it will not read /write any data to from the PLC device. 
Kindly also find the help document on this IODeviceControl function.
Was this helpful?
What can we do to improve the information ?