Technical FAQs

Ask a Question

Could we use Modbus and IEC61850 protocol with same Connuxium Ethernet Switch for using both protocol at the same time.

A managed switch will work on the network connection instead of the specific protocol. So you can use both protocols at a time with our Connexium switches, only you need to take care that the switch that you have selected will be having the management of RSTP for network redundancy. 
In  Connexium switch range you can select any of these TSCESM063F2CS1, TSCESM083F23F1, TSCESM063F2CU1 part numbers for this application. 
Was this helpful?
What can we do to improve the information ?