Technical FAQs

Ask a Question

How to resolve the #BAD error while communicating Vijeo Citect with PM870 meter using EGX100. Is there any specific setting need to be done in meter side.

There is no seperate settings were required in meter for communication with Vijeo Citect SCADA only you need to try communication of Vijeo Citect SCADA with PM870 meter by adding the following INI paramters in Vijeo Citect SCADA or try changing the variable tag scaling : 

1 [MODNET]InitVar = 40001 or any address register that you want to read. 

2. [MODNET]InitVarType = 3 

3, [MODNET]FloatMode = 1 
Was this helpful?
What can we do to improve the information ?