Technical FAQs

Ask a Question

Is it possible to increase frequency to 100 Hz on Altivar 71 drive.

Yes, it is possible to increase frequency to 100 Hz. for this, following parameter is required to change:
tFr[Max frequency]=>100 Hz
HSP[High speed]=>100 Hz

Note: It is possible to increase output frequency up to maximum 500Hz.
Was this helpful?
What can we do to improve the information ?