Technical FAQs

Ask a Question

What is the response time to reach frequency reference on Altivar 71 drive.

Regarding response time of ATV71 drive, it depends on Acceleration time (ACC) and Rated motor freq. (FrS). 

Example: if FrS =>50Hz and ACC =>60 Sec 
Frequency reference => 50 Hz. 
Then after run command, it will take 60 sec to reach 50Hz. 

Example: if FrS =>50Hz and ACC =>60 Sec 
Frequency reference => 30 Hz. 
Then after run command, it will take 36 sec [(60x30)/50] to reach 30Hz.
Was this helpful?
What can we do to improve the information ?