Technical FAQs

Ask a Question

What is the maximum inrush current (peak) for ABL6TS250U transformer.

The maximum inrush current (peak) for this type of transformer is 280Ap and depends on the switching off/on point in time. 
Recommended protection for short circuit and overload is the combination of: 
230V Input: GV2 RT 16 and C60N 24573 (1-pol) / 24525 (2-pol) 
400V Input: GV2 RT 16 and C60N 24525 (2-pol) 
Was this helpful?
What can we do to improve the information ?