Technical FAQs

Ask a Question

What could be the possible causes and solution to display is blank after applying control power to the PowerLogic PM5000 series power meter.

Possible Causes:
The power meter may not be receiving the necessary power.
The display may have timed out.

Possible Solutions:
Verify that the power meter line and terminals are receiving the necessary power.
Verify that the heartbeat LED is blinking.
Press a button to see if the display timed out.
Was this helpful?
What can we do to improve the information ?