Technical FAQs

Ask a Question

List Standard 1-Second Over/Under Alarms for PowerLogic PM5100 series power meter.

Following is the list of Standard 1-Second Over/Under Alarms for PowerLogic PM5100 series power meter;

01 Over Current, Phase
02 Under Current, Phase
03 Over Current, Neutral
04 Over Current, Ground
05 Over Voltage, L-L
06 Under Voltage, L-L
07 Over Voltage, L-N
08 Under Voltage L-N
09 Over kW
10 Over kVAR
11 Over kVA
12 Lead PF, True
13 Lag PF, True
14 Lead PF, Disp
15 Lag PF, Disp
16 Over kW Dmd, Pres
17 Over kW Dmd, Last
18 Over kW Dmd, Pred
19 Over kVAR Dmd, Pres
20 Over kVAR Dmd, Last
21 Over kVAR Dmd, Pred
22 Over kVA Dmd, Pres
23 Over kVA Dmd, Last
24 Over kVA Dmd, Pred
25 Over Frequency
26 Under Frequency
27 Over Voltage Unbal
28 Over Voltage THD
29 Phase Loss
Was this helpful?
What can we do to improve the information ?