Technical FAQs

Ask a Question

If user want to set the Analoge output of PM8M2222 to follow measurement called "frequency" which modbus register to be assigned in REG parameter.

If user want to set the Analoge output of PM8M2222 to follow "frequency", user will have to assigned the modbus register 1180 in REG parameter.
Was this helpful?
What can we do to improve the information ?