Technical FAQs

Ask a Question

Is it possbile to connect two PM8M2222 back to back on back side of PM800 series meter.

Yes, you can connect two PM8M2222 back to back on back side of PM800 series meter.

Attached you will find an I/O installation Manual that explains the Supply Voltage considerations for the PM8 meter. 
Was this helpful?
What can we do to improve the information ?