Technical FAQs

Ask a Question

How to assigning channel names in EGX300 I/O data basic reading screen adapted for Acti 9 Smartlink.

A specific name can be assigned to each channel. The procedure is as follow;

1. On the I/O data (basic readings) screen, click on Channel Names.
2. Click on the channel name to be changed.
3. Type in the new channel name.
  The number of characters is limited to 10.
4. Repeat steps 2 and 3 for all the channel names to be changed.
5. Click on the Apply button
Was this helpful?
What can we do to improve the information ?