Technical FAQs

Ask a Question

Is Modicon Quantum is complied with RFI protection and environmental standards.

Yes, Modicon Quantum is complied wit RFI Protection and environmental standards as per the IEC61000-4-3 and IEC1000-4-3 standards.Refer the attached documents.
Was this helpful?
What can we do to improve the information ?