Technical FAQs

Ask a Question

How to do Graphic Representation of Consumption in EGX300 adapted for Acti 9 Smartlink if impulse counters have been configured.

How to do Graphic Representation of Consumption in EGX300 adapted for Acti 9 Smartlink if impulse counters have been configured.

If impulse counters have been configured, consumption can be displayed in graphic form. The procedure is as follows:

1. In the Monitoring page, click on Device Logging.
2. In the Device drop-down menu, select Acti 9 Smartlink.
3. To select the values to be displayed, press the New Value(s) button.
4. Choose the values to be displayed and press the Apply button.
5. Use the mouse to select an area to be enlarged.

The illustration below gives an example of graphic representation of the meter consumption:
Was this helpful?
What can we do to improve the information ?