Technical FAQs

Ask a Question

In which BOX PC we can able to connect to a monitor with 1980 x 1200 resolution.

This resolution of 1920 x 1200 pixels will be available in S-BOX (Universal Range) part number HMIBSUCND1W01
Was this helpful?
What can we do to improve the information ?